40 Topic(s)
Part number: SXWTBIOW110002
Input modules support a single electrical type, such as digital or universal inputs. The available input modules include the following:
By adding a variety of Central IO and power supply modules, you can use the AS-P and AS-P-3 servers to tailor the Intelligent Building Management System to your unique requirements.
This Central IO module is a universal input, 16-channel I/O module. You can use the universal inputs for any mix of temperature, pressure, flow, status points, and similar inputs. You can also make adjustments for various sensor types using the available pull-up resistors.
You can wire a terminal base prior to installing an electronics module.
This section outlines the recommended cables and wires, specifying the appropriate wire sizes and lengths for the Central IO modules.
The terminal bases are used for SpaceLogic devices that are based on the patented two-piece design. The terminal base provides the I/O bus to the electronics module installed on the terminal base as well as to the SpaceLogic device installed to the right (next terminal base in the chain).
The Status LED on the front of the automation devices changes color and flashes to indicate the status of the device.
The EcoStruxure Building Operation software supports the major communication protocols in building automation and security management.
You print an I/O wiring list for the I/O bus that describes which I/O points are associated with each I/O module. You use the printed copy of this list to help wire the I/O bus network.