39 Topic(s)
Part number: SXWTBIOW110002
By adding a variety of I/O and power supply modules, you can use AS-P or Automation Server to tailor the Intelligent Building Management System to your unique requirements.
The Status LED on the front of the SmartStruxure devices changes color and flashes to indicate the status of the device.
The terminal bases are used for SmartStruxure devices that are based on the patented two-piece design. The terminal base provides the I/O bus to the electronics module installed on the terminal base as well as to the SmartStruxure device installed to the right (next terminal base in the chain).
Building Operation supports the major communication protocols in building automation and security management.
You print an I/O wiring list for the I/O bus that describes which I/O points are associated with each I/O module. You use the printed copy of this list to help wire the I/O bus network.
You print labels to identify I/O channels on the placard of an I/O module much the same way you label circuits on an electrical panel. You accept the default names for the I/O point labels or customize the I/O point names for your own application.
You perform the following steps to power up a device.
The wiring recommendations provide guidance regarding wiring of the I/O modules and the SmartStruxure server devices.
You can wire a terminal base prior to installing an electronics module.