earth_america
user_standard Log on
action_search_stroke
earth_america

UI-8/DO-FC-4

Refine your search
arrow2_down
Refine your search

39 Topic(s)

Hardware Installation

Part number: SXWTBIOW110002

Concept

By adding a variety of I/O and power supply modules, you can use AS-P or Automation Server to tailor the Intelligent Building Management System to your unique requirements.

Concept

The wiring recommendations provide guidance regarding wiring of the I/O modules and the SmartStruxure server devices.

How to

You can wire a terminal base prior to installing an electronics module.

Concept

The terminal bases are used for SmartStruxure devices that are based on the patented two-piece design. The terminal base provides the I/O bus to the electronics module installed on the terminal base as well as to the SmartStruxure device installed to the right (next terminal base in the chain).

User Interface

The Status LED on the front of the SmartStruxure devices changes color and flashes to indicate the status of the device.

Concept

Building Operation supports the major communication protocols in building automation and security management.

How to

You print an I/O wiring list for the I/O bus that describes which I/O points are associated with each I/O module. You use the printed copy of this list to help wire the I/O bus network.

How to

You print labels to identify I/O channels on the placard of an I/O module much the same way you label circuits on an electrical panel. You accept the default names for the I/O point labels or customize the I/O point names for your own application.

How to

You perform the following steps to power up a device.