earth_america
user_standard Log on
action_search_stroke
earth_america

UI-8/DO-FC-4

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

42 Topic(s)

Hardware Installation

Part number: SXWTBIOW110002

Concept

For Central IO modules with outputs, the following components on the front provide control of the output channels:

Concept

By adding a variety of Central IO and power supply modules, you can use the AS-P and AS-P-3 servers to tailor the Intelligent Building Management System to your unique requirements.

How to

You can wire a terminal base prior to installing an electronics module.

Concept

This section outlines the recommended cables and wires, specifying the appropriate wire sizes and lengths for the Central IO modules.

Concept

The terminal bases are used for SpaceLogic devices that are based on the patented two-piece design. The terminal base provides the I/O bus to the electronics module installed on the terminal base as well as to the SpaceLogic device installed to the right (next terminal base in the chain).

User Interface

The Status LED on the front of the automation devices changes color and flashes to indicate the status of the device.

Concept

The EcoStruxure Building Operation software supports the major communication protocols in building automation and security management.

How to

You print an I/O wiring list for the I/O bus that describes which I/O points are associated with each I/O module. You use the printed copy of this list to help wire the I/O bus network.

How to

You print labels to identify I/O channels on the placard of an I/O module much the same way you label circuits on an electrical panel. You accept the default names for the I/O point labels or customize the I/O point names for your own application.