1235 Topic(s)
The EcoStruxure Building Operation software supports the major communication protocols in building automation and security management.
You print an I/O wiring list for the I/O bus that describes which I/O points are associated with each I/O module. You use the printed copy of this list to help wire the I/O bus network.
You print labels to identify I/O channels on the placard of an I/O module much the same way you label circuits on an electrical panel. You accept the default names for the I/O point labels or customize the I/O point names for your own application.
The EcoStruxure Building Operation software gives you a number of functions to monitor and manage your facilities.
A meter object defines and maps energy values from devices so that they can be used by other objects in the building management system.
A meter group represents all the meters a customer or tenant is using.
The change of value trend log records the variable each time the difference between the current value and the last log value exceeds the delta. Use the change of value trend log to, for example, record a variable that has an unequal oscillation.
An alarm compares the value from a monitored variable with the conditions of the alarm. Different types of alarms handle different types of variables and different forms of evaluation.
Listed below are the System Alarms with IDs that begin with the letters E-L.
You remove devices from the allowlist when you no longer want them to communicate with the field server.