WebReports

172 Topic(s)
Use the filters below to limit the number of search hits.
Functionality
Information Type
Topic
Modified
Rating
5/13/2019
.NET Framework 4.7
You must install .NET Framework 4.7 before you can successfully install WebReports.
5/13/2019
Features Dialog Box for Windows Server 2012
Use the Features dialog box to select the .NET Framework 3.5 and .NET Framework 4.x features for installation. The features are required for the WebReports installation, and it is recommended that you install the services before you install SQL Server.
5/13/2019
WebReports Installation Overview
EcoStruxure Building Operation WebReports is installed using an installation package. Before you install WebReports, you must ensure that the computer on which you want to install WebReports (the Reports Server) meets the hardware and software requirements for WebReports, and that you have installed or enabled certain prerequisite items of software. These requirements are covered in the installation workflow (introduced in this topic).
5/13/2019
WebReports Installation WorkFlow
The WebReports installation workflow provides a guide to overall WebReports installation.
5/13/2019
Windows Roles and Features
The WebReports installation requires you to select certain roles and services to install on the Application Server and the Web Server (IIS), and to install .NET Framework 3.5 and .NET Framework 4.x features. You install these roles and features using the Server Manager in Windows Server 2008, Windows Server 2012, Windows Server 2012 R2, or Windows Server 2016. For Windows 7, Windows 8.1, and Windows 10, you configure the roles and features using Control Panel. It is recommended that you install these roles and features before you install SQL Server.
5/13/2019
5/13/2019
WebReports Installer and WebReports Components
The WebReports Installer is a custom installer program that performs installation, prevalidation, and configuration of WebReports components. The WebReports Installer is delivered in an installation package, and the installation package has the format WebReports-x.x.xxxxx.xxxx.exe. When you run the installation package, the WebReports Installer and accompanying files are placed in /Program Files (x86)/Schneider Electric EcoStruxure/Building Operation WebReports Installation by default. The WebReports Installer will automatically run to install the WebReports when you run the installation package.
5/7/2019
SQL Server
Before you can install WebReports successfully, it is imperative that the SQL Server has been installed with a particular group of settings.
5/6/2019
Engineering Tools Overview
You engineer your system using the engineering tools.
5/2/2019

Product version

Language