374 Topic(s)
Use the Building Operation WebStation window to log on to WebStation.
You change the filter conditions to narrow what is displayed in the Alarms pane, Events pane, Alarm View, or Event View.
You sort on alarms and events to get a better overview in the Alarms View or Events View.
You select fields in the Alarm view or Event view to display information regarding alarms and events.
When you force a value, you override all input from the system. For example, if a schedule is set to enable a device at 09:00, but you want to enable it at 08:00, you can force the enablement at 08:00.
You can filter on a specific value in an alarm view in WebStation.
Use the Select Object dialog box to select the objects you want to add to the widget.
You add schedules to a Multi schedule viewer to get an overview and be able to edit several events from the same Multi schedule viewer.
You create a Multi schedule viewer to view and edit several schedules at the same time.