405 Topic(s)
Use the Building Operation WorkStation window to log on to WorkStation.
System alarms monitor system entities, such as online status for field servers or field devices. The system alarms are generated by the EcoStruxure Building Operation software. Users cannot create new system alarms. The possible causes of a system alarm are gathered in an enumeration called System alarm ID. When a system alarm is triggered, the cause of the alarm is indicated in the System alarm ID column in the Alarms pane or Alarm View. Some system alarms have additional information in the Alarm text column.
When you force a value, you override all input from the system. For example, if a schedule is set to enable a device at 09:00, but you want to enable it at 08:00, you can force the enablement at 08:00.
There are a number of different clients, servers, and features that requires licenses to operate.
Licenses are needed for EcoStruxure Building Operation products and features that run on Windows.
Use the Xenta Schedule Editor to view and configure weekly events and exception events for a Xenta schedule.
Use the Xenta Schedule dialog box to edit the exception start and stop date, time interval, and weekday of a weekly or exception event.
You can open documents stored on an EcoStruxure BMS server using the default program associated with the file type. For example, a txt-file opens Notepad and a ppt-file opens PowerPoint.