earth_america
user_standard Log on
action_search_stroke
earth_america

WorkStation

Refine your search
arrow2_down
Refine your search
Ok
Ok
Ok

402 Topic(s)

Concept

You change the filter conditions to narrow what is displayed in the Alarms pane, Events pane, Alarm View, or Event View.

Specifications

Concept

​System alarms monitor system entities, such as online status for field servers or field devices. The system alarms are generated by the EcoStruxure Building Operation software. Users cannot create new system alarms. The possible causes of a system alarm are gathered in an enumeration called System alarm ID. When a system alarm is triggered, the cause of the alarm is indicated in the System alarm ID column in the Alarms pane or Alarm View. Some system alarms have additional information in the Alarm text column.

Concept

When you force a value, you override all input from the system. For example, if a schedule is set to enable a device at 09:00, but you want to enable it at 08:00, you can force the enablement at 08:00.

User Interface

Use the Calculated Exception view in the Schedule Event Properties dialog box to schedule recurring exceptions.

User Interface

Use the Add/Remove Columns dialog box to add or remove columns to the Search View.

Concept

Every time an alarm changes its state, such as from alarm state to reset state, an event is written in the event log and shown in the Events pane in WorkStation. You can disable state-change logging if you are only interested in the current alarm status. For example, you want to present the current alarm status in a graphic and do not care about the event history.

How to

You add a cause note to an alarm to let others know what caused the alarm.

How to

You add an exception event to configure an exception that is to apply instead of a scheduled weekly event for a single date, date range, or a time pair.

How to

You add an object to the Watch pane or a Watch View to dynamically monitor its property changes.