earth_america
user_standard Log on
action_search_stroke
earth_america

Communication Configuration

Central IO
BACnet/IP devices
RP Controller Expansion Modules
SE8000/VT8000
Touchscreen Room Controller
In-Room Door Lock Gateway
ION
BACnet
LonWorks
Modbus
KNX
Zigbee
IoT
OPC UA
Web Services
SmartDrivers
Engage Mobile Application
RP-C-RC-BLE
Xenta
MNL
MNB
b3
Infinet
NETWORK 8000
I/NET
MicroNet
Sigma
Cloud Agent
Refine your search
arrow2_down
Refine your search

131 Topic(s)

Concept

SpaceLogic Sensors are a family of living space sensors designed for BACnet/IP controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the BACnet/IP controller.

Concept

You can reset and restart the RP controllers in different ways depending on how long you press the reset button. The resets and restarts can affect the retention of values after restart based on the retain levels configured for the variables.

Concept

You can reset and restart the MP controllers in different ways depending on how long you press the reset button. The resets and restarts can affect the retention of values after restart based on the retain levels configured for the variables.

Concept

You can reset and restart the IP-IO and RP-IO modules in different ways depending on how long you press the reset button. The resets and restarts can affect the retention of values after restart based on the retain levels configured for the variables.

Concept

These hardening guidelines applies to Cloud Agent.

Concept

You must configure the DIP switches as part of the commissioning process for the RP and MP controllers and RP-IO modules that only support BACnet MS/TP communications.

Specifications

How to

​In WorkStation, you add one or more Xenta OP operator panels to the Building Operation network.

User Interface

Use the Advanced Commands submenu to execute functions on the selected LonWorks device or Xenta device.

Concept

The EcoStruxure Building Operation software supports the major communication protocols in building automation and security management.