earth_america
user_standard Log on
action_search_stroke
earth_america

Localization

Refine your search
arrow2_down
Refine your search

56 Topic(s)

Concept

Numeric objects and some property types in EcoStruxure Building Operation support configurable units of measure. In certain object types, the unit is predefined and cannot be modified. The configured unit applies to the value stored in the server.

Concept

​Consistent date and timestamping across a network is critical for system wide access control, security, communications, scheduling, alarms, and events. Network time uses the NTP protocol that provides the correct current UTC time.

How to

You display the server time using a Time Stamp Value object when you want to display the local time for a server in another time zone than the client time zone.

User Interface

Use the Time tab to configure the network time server addresses or establish a lead and shadow relationship on EcoStruxure BMS servers.

How to

You define and change the unit and its prefix for a value to ensure that the value is correct calculated.

How to

You add a language to WebStation so that the user can change to this language.

User Interface

Use the Add or remove languages dialog box to add or remove language that can be selected in WebStation.

User Interface

Use the Date and time tab to configure the server to use an external NTP server and to configure a time zone.

Concept

The EcoStruxure Building Operation software handles values and numbers with the highest ​precision. By default, the unit of a value is converted according to the regional settings of the user’s operating system.

Concept

​In WorkStation, all times are by default displayed in local time. This means that a time, independent of its source, is displayed in the same time zone as the operating system on which WorkStation is installed. By configuring the operating system time and time zone settings, you configure how times are displayed in WorkStation. For more information, please refer to the manufacturer’s manual for the operating system.