162 Topic(s)
The Trend Log Comparison report provides a way for you to compare the output of the trend logs associated with a data point, such as the kilowatts for a power meter. The report provides similar reporting as the Trend Chart, however, you can export the report, schedule the report, and run the report using a Web browser and without access to WorkStation.
The Schedule Report Activity report provides information about WebReports Schedules. You can use the report to identify whether a Reports schedule ran successfully, the number of times the schedule ran, and the average amount of time, in seconds, that the schedule ran.
The Database Schema Report provides information about the Reports database on the Reports Server. You can use the report to look up the names, data types, and descriptions of the fields used in the database tables for WebReports. Typically, you need this information when building SQL statements to create your own reports using Microsoft Report Builder.
The Alarm Amount by Type report provides information about the number of triggered alarms and organizes the information by alarm type, such as Change of State Alarm and Out of Range Alarm. You can use the report to track the greatest number of triggered alarms by alarm type.
The Alarm Amount by Category report provides information about triggered alarms and organizes the information by alarm categories. Before you can generate report output for this report, you need to set up alarm categories in WorkStation and link alarms to the alarm categories. For example, you can set up door alarm categories or cooling alarm categories. You can then use the report to determine the problematic areas in your buildings such as the door alarms.
The Activities Per User report provides information about some of the user activities for a particular user account. You can use the report to audit user activities such as creating and deleting objects, and completing successful logons.
To uninstall WebReports, you use the Windows Add Remove Program tool. The Windows Add Remove Program tool permanently removes the Building Operation product from the computer or server.
Building Operation WebReports is installed using an installation package. Before you install WebReports, you must ensure that the computer on which you want to install WebReports (the Reports Server) meets the hardware and software requirements for WebReports, and that you have installed or enabled certain prerequisite items of software. These requirements are covered in the installation workflow (introduced in this topic).
You must install .NET Framework 4.5 before you can successfully install WebReports.
You configure the SQL server memory to ensure that the reports do not take more time to get generated.