74 Topic(s)
Semantic is based on ontologies.
You can change the class of a semantic item.
You enable semantic for EWS when you want to expose semantic information to an EWS client.
You upload ontologies on your system so that the correct ontologies are used on the semantic database.
Update the semantic model if you have added alarms or trend logs to an EBO object that already have a relation to a semantic item. When you update the semantic model the alarm and trend log is added to the semantic model.
You can create a semantic repository for each tenant. You do this in a system with multi tenants where you do not want the tenants to share their semantic information.
Use the Tenant Repository dialog box to create a semantic database user and the content this user has access to.
Use the Tenant Repositories dialog box to add and edit tenant repository.
Use the semantic tagging filter buttons to filter on the semantic classes Point, Equipment, System, and Location.
Use this workflow to create and configure tenant repositories.