earth_america
user_standard Log on
action_search_stroke
earth_america

Touchscreen

Refine your search
arrow2_down
Refine your search

20 Topic(s)

Concept

SpaceLogic Sensors are a family of living space sensors designed for BACnet/IP controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the BACnet/IP controller.

How to

In the SpaceLogic Sensor Touchscreen Display model, you change the occupancy mode to tell the control system that the room is occupied or unoccupied. You do so by enabling the Display object Occupancy override property. Depending on the control system programming, it may respond in various ways including changing the active setpoint from unoccupied to occupied, turning on the lights, and/or starting a timer that expires when the system becomes unoccupied again.

Concept

The Touchscreen Display model provides a menu-driven interface with a front menu and a functions menu screen that you configure through EcoStruxure Building Operation.

Concept

SpaceLogic Sensor devices are modular and are ordered in two parts: the sensor base and the cover. Four SpaceLogic communicating sensor base models are available as well as a variety of covers.

How to

In the SpaceLogic Sensor Touchscreen Display model, you select the degree type in order to see the temperature in the preferred units of the room occupant. You enable this feature by choosing the Display object Allow temperature unit changes property, followed by the Temperature units property and its Fahrenheit or Celsius option.

How to

In the SpaceLogic Sensor Touchscreen model, you select the fan speed to change the air flow in the designated living space. You enable this feature using the Display object Allow fan speed changes property.

How to

You can program lighting control to create special scenes that illuminate an area based on the time of day, such as dimming the lights with the click of the night light button.

Concept

SpaceLogic Sensor include blank cover and occupancy sensor-only cover models, as well as several models with pushbutton or display-driven user interfaces that allow you to control temperature, occupancy, overrides, and a variety of other settings in a designated living space.

User Interface

Use the SpaceLogic Sensor Touchscreen Display model front menu screen to view and change the current settings and advance to the functions menu screen.

User Interface

Use the SpaceLogic Sensor Touchscreen Display model functions menu to perform a variety of tasks. For example, with the functions menu configured as shown, you can perform the following tasks: