1071 Topic(s)
You start Software Administrator to be able to configure the port settings of the Enterprise Server or Enterprise Central.
You need debug information to analyze why the crash information is not available on Connect storage server. Debug information is retrieved from the crash log files.
You configure Windows Firewall for Connect Agent to ensure that the system and crash information is available on Connect storage server.
You install a Twisted Pair Adapter on a flat surface inside a cabinet to properly fasten the device and to allow for sufficient ventilation.
You install a Twisted Pair Adapter on a DIN rail inside a cabinet to properly fasten the device and to allow for sufficient ventilation.
You set an EcoStruxure BMS server to password reset mode so that you can create a new password if the old one was forgotten.
You edit your Installation and System Information to update your contact information.
You connect to an Enterprise Server or Enterprise Central so that you can set the servers to reset mode.
You clear the list of the display names and IP addresses of servers when you do not need the contents anymore.
You configure an automation server to use 802.1X Protected EAP to increase the security.