51 Topic(s)
You start Software Administrator to be able to configure the port settings of the Enterprise Server or Enterprise Central.
Ensuring the EcoStruxure Building Management integration is installed securely is key to the overall security envelope of the building. The following integration security configurations need to be considered to ensure the overall security meets “best practice” standards.
You configure an automation server to use 802.1X Protected EAP to increase the security.
You configure an automation server to use 802.1X EAP TLS to increase the security.
You configure an automation server to use 802.1X MD5 to increase the security.
You can reset the administrator password on your EcoStruxure Building Operation servers if you, for example, have locked yourself out.
Click to get information on the Edit Connection and Add Server dialog boxes in Device Administrator.
You add the IP addresses of the devices that are allowed to communicate with the automation server or the FDP server to the firewall whitelist. This helps prevent connection attempts from unauthorized devices.
These hardening guidelines applies to the EcoStruxure Building Operation software products and the EcoStruxure BMS server products.
You configure the SSL communication to increase the security of your system.