earth_america
user_standard Log on
action_search_stroke
earth_america

AS-P Smoke Control

Refine your search
arrow2_down
Refine your search

44 Topic(s)

Hardware Installation

Specifications

Hardware Installation

Concept

The wiring of the I/O terminals varies based on the type of I/O provided on the various modules. There are many modules that present differing combinations of the same I/O types. In describing the wiring of the I/O modules, the wiring descriptions that follow are based first on I/O type to avoid duplicating the I/O wiring information described for each of the module models.

Concept

MS/TP BACnet Controllers provide the outputs to actuate the dampers and control the fans for the system when the equipment is distributed throughout a facility (most instances). The MS/TP BACnet controllers for the smoke control system are listed here.

Concept

The Firefighter’s Smoke Control Station (FSCS) is a custom-designed control and display panel tailored for each specific project. The FSCS panel provides the ability to observe the current state of all of the equipment in the smoke control system. The panel allows authorized users to override the On/Off or Open/Closed state of the system equipment. The FSCS design is unique to each project with its objective being to present a graphic presentation of the location and function of the various system elements. LED indicators are positioned on or next to equipment images and illuminate to show the current equipment state. A fault LED illuminates if the equipment fails to achieve the state directed by the automated smoke response or the override from the FSCS panel. Switches positioned on the panel next to the applicable equipment images are used to override the current state (such as open or close a damper, or direct a fan to run or stop).

Concept

The UL 864 listed MNA-FLO-1 enclosure is a 2.75-inch deep (69.85 mm) box designed for use with VAV controllers.

How to

You mount UL 864 Smoke Control enclosures on any hard surface, such as metal, wood, brick, mortar, and thin drywall (hollow wall). Be sure to always mount the enclosure indoors.

Concept

The following transformers are approved for the SmartStruxure Solution Smoke Control System.

Concept

You should ensure that you have the proper diameter mounting hardware and anchoring system before mounting the UL 864 Smoke Control enclosures.