1570 Topic(s)
These hardening guidelines applies to Cloud Agent.
The output override function allows you to manually override outputs. This function can be used for testing, commissioning, and maintenance of equipment.
The AS-P server offers enhanced processor performance, increased memory size, dual Ethernet ports, and high-speed USB interfaces. The AS-P server is a Schneider Electric manufactured embedded device that generally serves as the lowest tier EcoStruxure BMS server within the EcoStruxure BMS. The AS-P controls and supervises equipment, typically HVAC equipment. AS-P servers use Central IO module with connected field devices, such as sensors and actuators, to do that.
You use an extended trend log to store records from a trend log. An extended trend log can be connected to a trend log or connected in a series to another extended trend log. Only one extended trend log can be connected to a trend log​ or another extended trend log.
You set an EcoStruxure BMS server to password reset mode so that you can create a new password if the old one was forgotten.
Ensuring the EcoStruxure Building Management integration is installed securely is key to the overall security envelope of the building. The following integration security configurations need to be considered to ensure the overall security meets “best practice” standards.
Use the Options dialog box to manage some local user settings.
Use the Building Operation WorkStation window to log on to WorkStation.
You use theDisplay Names and IP Addresses of Servers drop-down list box to add, edit and delete the display names of the server addresses. You also use it to export, import and delete lists of the display names and IP addresses of servers.