earth_america
user_standard Log on
action_search_stroke
earth_america

BACnet/IP Devices

RP-C
RP-V
MP-C
MP-V
IP-IO
RP-IO
MP-C Smoke Control
MP-V Smoke Control
IP-IO Smoke Control
Refine your search
arrow2_down
Refine your search

505 Topic(s)

Hardware Installation

Part number: SXWRCF16C10001

Concept

This section provides information on the external connectors that are required for the power supply input, outputs, and digital inputs of the RP controller expansion modules.

Concept

The CRS-HH-REL-10 relay module connects to the RP controllers and enables the control of lights and blinds.

Specifications

Specifications

Specifications

Concept

SpaceLogic Sensors are a family of living space sensors designed for BACnet/IP controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the BACnet/IP controller.

Concept

The KNX Modbus gateway RP-C-EXT-KNX connects to the RP-C controllers and provides an interface between the controller and KNX devices such as push-buttons, sensors, and control units for lights, blinds, and room temperature.

Concept

The IP-IO module comes in three models with different I/O point count and different I/O point types.

Concept

The output override function allows you to manually override outputs. This function can be used for testing, commissioning, and maintenance of equipment.