earth_america
user_standard Log on
action_search_stroke
earth_america

Central IO Modules

UI-8/AO-4 v2
UI-8/AO-V-4 v2
UI-8/DO-FC-4 v2
UI-16 v2
DI-16
RTD-DI-16
AO-8
AO-V-8
DO-FA-12
DO-FC-8
UI-8/AO-4
UI-8/AO-V-4
UI-8/DO-FC-4
UI-16
Refine your search
arrow2_down
Refine your search

71 Topic(s)

Concept

Input modules support a single electrical type, such as digital or universal inputs. The available second version (v2) input modules include the following:

Concept

The second-generation (v2) Central IO modules feature several enhancements over the first-generation models, including faster processor performance and higher-resolution A/D converters for universal inputs. Additionally, the v2 module design has been updated to better align with the DIN 43880 standard by removing the previously high shoulder height. By adding a variety of Central IO and power supply modules, you can use the AS-P server to tailor the Intelligent Building Management System to your unique requirements.

Specifications

Hardware Installation

Part numbers: SXWUI16XX10002, SXWUI8D4X10002, SXWUI8D4H10002, SXWUI8A4X10002, SXWUI8A4H10002, SXWUI8V4X10002, SXWUI8V4H10002

Hardware Installation

Part number: SXWTBIOW110002

Concept

This Central IO module is a universal input, 16-channel I/O module. You can use the universal inputs for any mix of temperature, pressure, flow, status points, and similar inputs. You can also make adjustments for various sensor types using the available pull-up resistors.

Concept

By adding a variety of I/O and power supply modules, you can use AS-P or Automation Server to tailor the Intelligent Building Management System to your unique requirements.

Concept

The UI-16 I/O module is a universal input, 16-channel I/O module. Each channel has a dedicated status two-color LED that provides local monitoring of digital, counter, and supervised input types. The front panel shows the module status LED and the I/O channel status LEDs.

Concept

Input modules support a single electrical type, such as digital or universal inputs. The available input modules include the following:

Concept

The wiring recommendations provide guidance regarding wiring of the I/O modules and the SmartStruxure server devices.