earth_america
user_standard Log on
action_search_stroke
earth_america

Enterprise Server

Refine your search
arrow2_down
Refine your search

884 Topic(s)

How to

You edit a backup rule on a SmartStruxure server to change the type of data that you want to back up. You can also set up this backup rule to follow a shadow schedule that references a lead schedule managed on another SmartStruxure server. 

How to

You create an out of reference range alarm to trigger an alarm when a variable, such as a temperature, differs from a reference value.

How to

You create an out of range alarm to trigger an alarm when a variable, such as a temperature, is not within its specified range.

How to

You create an interval trend log to record a value of a variable at specified and regularly occurring increments of time.

How to

You create an extended trend log to store log records for a longer period of time and free up memory in the SmartStruxure server device. Extended trend logs are also required for generating reports using Building Operation WebReports.

How to

You configure the Archive settings and schedule on the Enterprise Server to automate the archiving process.

How to

You use the meter trend log to record the value of a meter and handle consumption calculations independent of meter rollover and meter exchange.

How to

You create a change of state alarm to trigger an alarm when a variable, such as a switch, is either true or false.

How to

You back up multiple SmartStruxure servers manually to copy and store data that is frequently updated.

Concept

​In WorkStation, all times are by default displayed in local time. This means that a time, independent of its source, is displayed in the same time zone as the operating system on which WorkStation is installed. By configuring the operating system time and time zone settings, you configure how times are displayed in WorkStation. For more information, please refer to the manufacturer’s manual for the operating system.