earth_america
user_standard Log on
action_search_stroke
earth_america

IP-IO

Refine your search
arrow2_down
Refine your search

99 Topic(s)

Concept

The IP-IO module comes in three models with different I/O point count and different I/O point types.

Concept

The IP-IO module is delivered with terminal blocks installed on the device. The IP-IO module uses pluggable terminal blocks, which are easy to install and remove from the device.

Specifications

How to

You wire the terminal blocks installed on the IP-IO module to connect I/O devices and power.

How to

You remove a terminal block from an IP-IO module in order to replace the module.

Hardware Installation

Part number: SXWMPCDSP10A01

Hardware Installation

Part numbers: SXWIPIOAA10A01, SXWIPIOBA10A01, and SXWIPIOCA10A01

How to

You install the terminal blocks on an IP-IO module to add or enable wiring for the device.

Concept

The IP-IO module has a built-in power supply designed to accommodate 24 VAC at 50/60 Hz or 24 to 30 VDC input power.

How to

You can select the Feedback option to rate your experiences and provide detailed information on the Commission mobile application.