125 Topic(s)
The IP-IO module comes in three models with different I/O point count and different I/O point types.
The output override function allows you to manually override outputs. This function can be used for testing, commissioning, and maintenance of equipment.
IP-IO-UIO5DOFA4 has 9 I/O points and the IP-IO module is equipped with four pluggable terminal blocks and one fixed terminal block.
IP-IO-UIO10 has 10 I/O points and the IP-IO module is equipped with four pluggable terminal blocks.
IP-IO-DI10 has 10 I/O points and the IP-IO module is equipped with four pluggable terminal blocks.
The IP-IO module is delivered with terminal blocks installed on the device. The IP-IO module uses pluggable terminal blocks, which are easy to install and remove from the device.
There are many different kinds of external devices from different vendors that can be connected to an EcoStruxure BMS.
The wiring recommendations provide guidance regarding wiring of the Central IO modules, automation servers, RP and MP controllers, IP-IO and RP-IO modules, RP controller expansion modules, Operator Display, and Twisted Pair Adapter.
This section provides recommendations on minimum wire sizes (cross-sectional areas) and maximum wire lengths for the wires connected to the screw terminals of Central IO modules, AS-B servers, RP and MP controllers, and IP-IO and RP-IO I/O modules. Recommendations on minimum wire sizes and maximum cable lengths for the various inputs and outputs of the different RP controller expansion modules and the KNX Modbus gateway are also provided. The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.
The Status LED on the front of the automation devices changes color and flashes to indicate the status of the device.