earth_america
user_standard Log on
action_search_stroke
earth_america

IP-IO

Refine your search
arrow2_down
Refine your search

125 Topic(s)

Concept

RP and MP controllers and I/O modules are devices that have three types of memory:

Concept

You can reset and restart the IP-IO and RP-IO modules in different ways depending on how long you press the reset button. The resets and restarts can affect the retention of values after restart based on the retain levels configured for the variables.

Specifications

Concept

The IP-IO module comes in three models with different I/O point count and different I/O point types.

Concept

The output override function allows you to manually override outputs. This function can be used for testing, commissioning, and maintenance of equipment.

Concept

IP-IO-UIO5DOFA4 has 9 I/O points and the IP-IO module is equipped with four pluggable terminal blocks and one fixed terminal block.

Concept

IP-IO-UIO10 has 10 I/O points and the IP-IO module is equipped with four pluggable terminal blocks.

Concept

IP-IO-DI10 has 10 I/O points and the IP-IO module is equipped with four pluggable terminal blocks.

Concept

The IP-IO module is delivered with terminal blocks installed on the device. The IP-IO module uses pluggable terminal blocks, which are easy to install and remove from the device.

Concept

The IP-IO module provides I/O expansion to your HVAC application over BACnet/IP and can share their I/O resources across applications running in automation servers, BACnet/IP controllers, or third-party systems. The IP-IO module can be installed near facilities in the field, away from the automation server or the BACnet/IP controller.