earth_america
user_standard Log on
action_search_stroke
earth_america

MP-V

Refine your search
arrow2_down
Refine your search

141 Topic(s)

Concept

The MP-V comes in two models with a different I/O point count and different I/O point mix.

Concept

MP-V-9A has nine I/O points and the controller is equipped with four pluggable terminal blocks.

Concept

MP-V-7A has seven I/O points and the controller is equipped with four pluggable terminal blocks.

Concept

The MP-V is delivered with terminal blocks installed on the device. The MP-V uses pluggable terminal blocks, which are easy to install and remove from the device.

Concept

There are few differences in hardware between different hardware versions of the MP-V models.

Concept

You must configure the DIP switches as part of the commissioning process for RP controllers that support MS/TP communications.

Concept

The wiring recommendations provide guidance regarding wiring of the Central IO modules, automation servers, RP and MP controllers, IP-IO modules, RP controller expansion modules, and Operator Display.

Concept

This section provides recommendations on minimum wire sizes (cross-sectional areas) and maximum wire lengths for the wires connected to the screw terminals of Central IO modules, AS-B servers, RP and MP controllers, and IP-IO modules. Recommendations on minimum wire size and maximum cable length for the digital inputs of the RP controller expansion modules, the DALI bus of the DALI light modules, the SMI Interface of the SMI blind modules, the Zigbee DALI and 0-10V modules, and the KNX Modbus gateway are also provided. The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.

User Interface

The Status LED on the front of the automation devices changes color and flashes to indicate the status of the device.

Concept

The I/O wiring recommendations provide guidance on what type of wires should be used for the different Central IO modules, AS-B server onboard I/O, RP and MP controller onboard I/O, and IP-IO modules, how to perform grounding, and how to connect different external devices to the inputs and outputs. This section also provides information on the external connectors required for the RP controller expansion modules. Always use the recommended cables and wires.