earth_america
user_standard Log on
action_search_stroke
earth_america

MP-V

Refine your search
arrow2_down
Refine your search

148 Topic(s)

Concept

SpaceLogic Sensors are a family of living space sensors designed for BACnet/IP controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the BACnet/IP controller.

Concept

You can reset and restart the MP controllers in different ways depending on how long you press the reset button. The resets and restarts can affect the retention of values after restart based on the retain levels configured for the variables.

Concept

RP and MP controllers and I/O modules are devices that have three types of memory:

Concept

You can reset and restart the IP-IO and RP-IO modules in different ways depending on how long you press the reset button. The resets and restarts can affect the retention of values after restart based on the retain levels configured for the variables.

Specifications

Concept

The MP-V comes in two models with a different I/O point count and different I/O point mix.

Concept

MP-V-9A has nine I/O points and the controller is equipped with four pluggable terminal blocks.

Concept

MP-V-7A has seven I/O points and the controller is equipped with four pluggable terminal blocks.

Concept

The MP-V is delivered with terminal blocks installed on the device. The MP-V uses pluggable terminal blocks, which are easy to install and remove from the device.

Concept

There are few differences in hardware between different hardware versions of the MP-V models.