earth_america
user_standard Log on
action_search_stroke
earth_america

MP-V

Refine your search
arrow2_down
Refine your search

149 Topic(s)

Specifications

Concept

SpaceLogic Sensors are a family of living space sensors designed for BACnet/IP controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the BACnet/IP controller.

Concept

The MP-V comes in two models with a different I/O point count and different I/O point mix.

Concept

MP-V-9A has nine I/O points and the controller is equipped with four pluggable terminal blocks.

Concept

MP-V-7A has seven I/O points and the controller is equipped with four pluggable terminal blocks.

Concept

The MP-V is delivered with terminal blocks installed on the device. The MP-V uses pluggable terminal blocks, which are easy to install and remove from the device.

Concept

RP and MP controllers and I/O modules are devices that have three types of memory:

Concept

There are few differences in hardware between different hardware versions of the MP-V models.

Concept

Concept

Ensuring the EcoStruxure Building Management integration is installed securely is key to the overall security envelope of the building. The following integration security configurations need to be considered to ensure the overall security meets “best practice” standards.