earth_america
user_standard Log on
action_search_stroke
earth_america

Operator Display

Refine your search
arrow2_down
Refine your search

153 Topic(s)

Concept

When an input, output or value in a connected device is configured to generate an alarm, Operator Display allows you to view and acknowledge the alarm. Inputs, outputs or values can be configured to generate an alarm when it is, for example, out of range or in a fault state.

Concept

The Schneider Electric EasyLogic and SpaceLogic hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, Central IO modules, automation servers such as AS-P-3, AS-P and AS-B servers, MP-C, MP-V, RP-C, and RP-V controllers, IP-IO and RP-IO I/O modules, RP controller expansion modules, remote control, KNX Modbus gateway, Bluetooth adapter, Wireless Adapter - Advanced, SpaceLogic Sensor devices, Advanced Display devices, and Operator Display devices.

Concept

The wiring recommendations provide guidance regarding wiring of the Central IO modules, automation servers, RP and MP controllers, IP-IO and RP-IO modules, RP controller expansion modules, Operator Display, and Twisted Pair Adapter.

Concept

It is important to perform the grounding correctly for the following reasons:

How to

You upgrade the firmware to access the latest Operator Display features and bug fixes.

User Interface

Use the Select a region screen to configure the time zone of Operator Display.

Concept

This section provides information on regulatory and agency compliance and approvals for the SpaceLogic Operator Display.

User Interface

Use the Select time zone screen to configure the time zone of Operator Display.

Concept

The wiring recommendations for the communication ports on the automation servers, RP and MP controllers, IP-IO and RP-IO modules, RP controller expansion modules, and Operator Display devices apply to wires and cables used for RS-485 communications, LonWorks communications, USB connections, Ethernet connections, sensor bus connections, room bus connections, and RP and MP controller Modbus network connections. Always use the recommended cables and wires.

Concept

SpaceLogic™ Operator Display is a touch-screen Human Machine Interface (HMI) for SpaceLogic controllers and servers, designed for local monitoring of building controllers in small and medium-sized buildings, as well as in large buildings with comprehensive building management systems. Operator Display is specifically designed for equipment rooms and it simplifies operations, service, and troubleshooting for System Integrators and Service Engineers, as well as for non-technical users (notably Facility Managers and Janitors).