earth_america
user_standard Log on
action_search_stroke
earth_america

RP-C

Refine your search
arrow2_down
Refine your search

294 Topic(s)

Hardware Installation

Part number: SXWRCF16C10001

Concept

This section provides information on the external connectors that are required for the power supply input, outputs, and digital inputs of the RP controller expansion modules.

Concept

The CRS-HH-REL-10 relay module connects to the RP controllers and enables the control of lights and blinds.

Concept

SpaceLogic Sensors are a family of living space sensors designed for BACnet/IP controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the BACnet/IP controller.

Concept

The KNX Modbus gateway RP-C-EXT-KNX connects to the RP-C controllers and provides an interface between the controller and KNX devices such as push-buttons, sensors, and control units for lights, blinds, and room temperature.

Concept

The RP-C-16A-M-24V model has 16 I/O points and the controller is equipped with 30 fixed screw terminals and a 3-position removable screw terminal block.

Concept

The RP-C-16A model has 16 I/O points and the controller is equipped with 30 fixed screw terminals.

Concept

The RP-C-12C model has 12 I/O points and the controller is equipped with 24 fixed screw terminals.

Concept

The RP-C-12B-M-24V model has 12 I/O points and the controller is equipped with 24 fixed screw terminals and a 3-position removable screw terminal block.

Concept

The RP-C-12B model has 12 I/O points and the controller is equipped with 24 fixed screw terminals.