27 Topic(s)
You install an RP controller expansion Insight-Sensor on an octagon junction box using the supplied mounting ring to properly fasten the Insight-Sensor to the junction box.
You install an RP controller expansion Insight-Sensor on a ceiling using the supplied mounting ring to properly fasten the Insight-Sensor on the ceiling.
You install an RP controller expansion Insight-Sensor into a dropped ceiling using the mounting springs to properly fasten the Insight-Sensor to a ceiling tile.
The wiring recommendations provide guidance regarding wiring of the Central IO modules, automation servers, RP and MP controllers, IP-IO and RP-IO modules, RP controller expansion modules, Operator Display, and Twisted Pair Adapter.
RP controller expansion modules have two types of memory, flash memory and RAM.
The RP controller expansion modules provide a range of devices that can be combined to form a connected room solution. The RP controller expansion modules are connected to the RP controller room bus and provide the RP controllers with I/O expansion and sensors that enable lighting and blind control.
You configure an RP controller expansion module into online maintenance mode to read diagnostics from the device and to upgrade the device with new firmware.
There is one LED on the RP controller expansion sensor modules. The LED is integrated with the Set button.
This section provides information on regulatory compliance and approvals for the RP controller expansion sensor modules of the Insight-Sensor model.
The RP controller expansion modules support different modes that can be used for maintenance purposes.