163 Topic(s)
The CRS-HH-REL-10 relay module connects to the RP controllers and enables the control of lights and blinds.
The RP-V-5C-M model has five I/O points and the controller is equipped with 11 fixed screw terminals and a 3-position removable screw terminal block.
The RP-V-5A model has five I/O points and the controller is equipped with 11 fixed screw terminals.
The RP-V-4A model has four I/O points and the controller is equipped with 11 fixed screw terminals.
The RP-V has fixed screw terminals for the power input, SSR outputs, and universal inputs/outputs. The RP-V-5C-M model also has a removable screw terminal block for connection to the BACnet MS/TP (RS-485) network.
The RP-V controller is available in two models that support both BACnet/IP and MS/TP communication. These two models offer two different combinations (sets) of the number of I/O points and types of I/O points. The RP-V controller also comes in a model that only supports BACnet MS/TP communication.
You must configure the DIP switches as part of the commissioning process for the RP and MP controllers and RP-IO modules that only support BACnet MS/TP communications.
You install an RP controller expansion Insight-Sensor on an octagon junction box using the supplied mounting ring to properly fasten the Insight-Sensor to the junction box.
You install an RP controller expansion Insight-Sensor on a ceiling using the supplied mounting ring to properly fasten the Insight-Sensor on the ceiling.
You install an RP controller expansion Insight-Sensor into a dropped ceiling using the mounting springs to properly fasten the Insight-Sensor to a ceiling tile.