162 Topic(s)
You can reset and restart the RP controllers in different ways depending on how long you press the reset button. The resets and restarts can affect the retention of values after restart based on the retain levels configured for the variables.
RP and MP controllers and I/O modules are devices that have three types of memory:
The CRS-HH-REL-10 relay module connects to the RP controllers and enables the control of lights and blinds.
The RP-V-5C-M model has five I/O points and the controller is equipped with 11 fixed screw terminals and a 3-position removable screw terminal block.
The RP-V-5A model has five I/O points and the controller is equipped with 11 fixed screw terminals.
The RP-V-4A model has four I/O points and the controller is equipped with 11 fixed screw terminals.
The RP-V has fixed screw terminals for the power input, SSR outputs, and universal inputs/outputs. The RP-V-5C-M model also has a removable screw terminal block for connection to the BACnet MS/TP (RS-485) network.
The RP-V controller is available in two models that support both BACnet/IP and MS/TP communication. These two models offer two different combinations (sets) of the number of I/O points and types of I/O points. The RP-V controller also comes in a model that only supports BACnet MS/TP communication.
You must configure the DIP switches as part of the commissioning process for the RP and MP controllers and RP-IO modules that only support BACnet MS/TP communications.