19 Topic(s)
The Twisted Pair Adapter can be installed on a DIN rail or other flat surface inside a cabinet. The device is recommended to be installed in a cabinet, unless local regulations allow an exception.
You install a Twisted Pair Adapter on a flat surface inside a cabinet to properly fasten the device and to allow for sufficient ventilation.
You install a Twisted Pair Adapter on a DIN rail inside a cabinet to properly fasten the device and to allow for sufficient ventilation.
Twisted Pair Adapter supports Ethernet over twisted pair cable networks.
SpaceLogic™ Twisted Pair Adapter - Ethernet (TPA-E) connects to the SpaceLogic BACnet/IP controller and automation server via Ethernet 10/100 Mbit (IEEE 802.3) and utilizes existing twisted pair cabling originally used for legacy serial and free topology protocols. This enables seamless integration of existing twisted pair networks into the IP-based infrastructure of the EcoStruxure Building Management System (BMS), reducing installation costs and simplifying the transition from legacy systems, such as LonWorks FTT-10 networks, to the EcoStruxure BMS network.
Part number: SXWTPAE10001
The operating modes are controlled by the M/T slide switch on the front of the adapter:
The Twisted Pair Adapter is equipped with the following connectors:
You restart the Twisted Pair Adapter to intialize the device.