earth_america
user_standard Log on
action_search_stroke
earth_america

UI-8/DO-FC-4 v2

Refine your search
arrow2_down
Refine your search

36 Topic(s)

Concept

The AS-P server offers enhanced processor performance, increased memory size, dual Ethernet ports, and high-speed USB interfaces. The AS-P server is a Schneider Electric manufactured embedded device that generally serves as the lowest tier EcoStruxure BMS server within the EcoStruxure BMS. The AS-P controls and supervises equipment, typically HVAC equipment. AS-P servers use Central IO module with connected field devices, such as sensors and actuators, to do that.

Concept

The second-generation (v2) Central IO modules feature several enhancements over the first-generation models, including faster processor performance and higher-resolution A/D converters for universal inputs. Additionally, the v2 module design has been updated to better align with the DIN 43880 standard by removing the previously high shoulder height. By adding a variety of Central IO and power supply modules, you can use the AS-P server to tailor the Intelligent Building Management System to your unique requirements.

Hardware Installation

Part numbers: SXWUI16XX10002, SXWUI8D4X10002, SXWUI8D4H10002, SXWUI8A4X10002, SXWUI8A4H10002, SXWUI8V4X10002, SXWUI8V4H10002

Hardware Installation

Part number: SXWTBIOW110002

Concept

For Central IO modules with outputs, the following components on the front provide control of the output channels:

Concept

This section outlines the recommended cables and wires, specifying the appropriate wire sizes and lengths for the Central IO modules.

Concept

There are many different kinds of external devices from different vendors that can be connected to an EcoStruxure BMS.

User Interface

The Central IO modules have the following status indicator LEDs on the front of the module:

Concept

The wiring recommendations provide guidance regarding wiring of the Central IO modules, automation servers, RP and MP controllers, IP-IO and RP-IO modules, RP controller expansion modules, Operator Display, and Twisted Pair Adapter.

How to

You can wire a terminal base prior to installing an electronics module.