earth_america
user_standard Log on
action_search_stroke
earth_america

WorkStation

Refine your search
arrow2_down
Refine your search

409 Topic(s)

How to

You log on to WorkStation to securely access the functions in the EcoStruxure BMS.

How to

You create an interval trend log to record a value of a variable at specified and regularly occurring increments of time.

Concept

You use interfaces to set up, manage and operate the EcoStruxure BMS on a daily basis.

Concept

A dashboard report is a report that processes fixed or predefined filtering criteria to generate report output.

Concept

You can open documents stored on an EcoStruxure BMS server using the default program associated with the file type. For example, a txt-file opens Notepad and a ppt-file opens PowerPoint.

Concept

WorkStation is your main interface to your EcoStruxure BMS. You use WorkStation to perform all work on a daily basis in the EcoStruxure BMS.

How to

You duplicate an EcoStruxure BMS server from a backup set using Restore when you want to reuse configuration data from a backup set in a standalone SmartX server.

Concept

You can add attachments to alarm objects, except System Information alarms. An attachment is a link pointing to an object in the system. When an alarm that has an attachment is triggered, a paperclip icon is displayed in the Alarms pane and Alarm Views. It is also possible to configure the attachment to display when the alarm is going from Normal to Alarm state.

Specifications

User Interface

Use the Rename object dialog box to rename an object.