earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Commission, MP-C, MP-V, RP-C, SpaceLogic Sensors
Functionalities: Engineering, BACnet/IP devices
Product version: 3.0, 3.1
8/28/2019

eCommission Bluetooth Adapter

The eCommission Bluetooth Adapter allows you to establish a Bluetooth connection to MP and RP Series controllers. You plug the Bluetooth Adapter into the corresponding SmartX Sensor to connect to the controller. The Adapter communicates with the SmartX IP controller over the sensor bus using an RS-485 cable. For more information, see Connecting SmartX Sensors to an MP Series Controller .

Notice

SMARTX SENSOR OR OTHER EQUIPMENT DAMAGE

  • Plug in the adapter with the button to the front.

  • Do not plug into any device other than a SmartX Sensor.

Failure to follow these instructions can result in equipment damage.

For more information, see eCommission SmartX Controllers Mobile Application Overview .

 
action_zoom_plus_stroke eCommission Bluetooth adapter connectivity
Figure: eCommission Bluetooth adapter connectivity

Connecting to a Controller with the eCommission Bluetooth Adapter

The Bluetooth Adapter allows you to establish a Bluetooth connection to MP and RP Series controllers. To connect to a device through the Bluetooth Adapter, a SmartX Sensor must be wired to the controller.

For more information, see Connecting to a Controller with the Bluetooth Adapter .

Changing the PIN of the eCommission Bluetooth Adapter

You change the PIN of the eCommission Adapter for best security practices. The Bluetooth Adapter PIN is engineered to a default code of 333666 and should be changed to a secure code before you perform device commissioning.

For more information, see Changing the PIN of the eCommission Bluetooth Adapter .

Updating the eCommission Bluetooth Adapter Firmware

You update the eCommission Bluetooth Adapter firmware to improve adapter performance.

For more information, see Updating the eCommission Bluetooth Adapter Firmware .

Performing a Factory Reset of the eCommission Bluetooth Adapter

You perform a factory reset on the eCommission Bluetooth Adapter to erase the current PIN.

For more information, see Performing a Factory Reset on the eCommission Bluetooth Adapter .

eCommission Bluetooth Adapter LED Functionality

The eCommission Bluetooth Adapter LED light displays different sequences to indicate the various functionality.

For more information, see Bluetooth LED Functionality .

  • eCommission SmartX Controllers Mobile Application Overview
  • Connecting to a Controller through Bluetooth
  • Changing the PIN of the eCommission Bluetooth Adapter
  • Updating the eCommission Bluetooth Adapter Firmware
  • Performing a Factory Reset on the eCommission Bluetooth Adapter
  • Bluetooth LED Functionality