earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server
Functionalities: Hardware
Product version: 2.0, 2.1, 3.0, 3.1
8/20/2020

Automation Server LEDs

arrow1_rotationStatus LED arrow1_rotationRS-485 LEDs arrow1_rotationEthernet LED arrow1_rotationLON LEDs

There are eight LEDs on the front panel of the Automation Server.

 
action_zoom_plus_stroke Automation Server LEDs

Automation Server LEDs

Table: The Eight LEDs

Function

Color

RS-485 A, Tx

Yellow

RS-485 A, Rx

Green

RS-485 B, Tx

Yellow

RS-485 B, Rx

Green

Ethernet, Link/Act/Speed

Green/Yellow

LON, Tx

Yellow

LON, Mode

Red

Status (Automation Server)

Green/Red

Note:

The Automation Server Ethernet and Status indicators comprise two LEDs (green/yellow and green/red respectively) in one structure. Normally, when one LED is lit, the other is not lit and vice versa, that is, the indicator will show one color at a time.

The LEDs indicate status of the Automation Server and the ongoing communication.

Status LED

The SmartX server Status LED indicates the condition of the device.

Table: SmartX Server Status LED Patterns

LED Patterns

Condition

Green, constant

Normal operation, status OK

Green, flashing (~1 Hz)

Device restarting, wait

Red, constant

Detected error, attention required

Red, flashing (~1 Hz)

Device operates, but a problem needs attention

Red/green, flashing (~1 Hz)

Firmware being downloaded, wait

Red/green, vague

Device firmware upgrade mode, wait

No light

No input power

RS-485 LEDs

The RS-485 (COM A and COM B) LEDs indicate the condition of the RS-485 communication.

Table: RS-485 LED Patterns

LED Patterns

Condition

Yellow, flashing (Tx)

Transmit data

Green, flashing (Rx)

Receive data

Ethernet LED

The Ethernet LED indicates the condition of the Ethernet communication.

Table: Ethernet LED Patterns

LED Patterns

Condition

Green, flashing

10 Mbit communication

Yellow, flashing

100 Mbit communication

LON LEDs

The LON LEDs indicate the condition of the LonWorks RS-485 communication.

Table: LON LED Patterns

LED Patterns

Condition

Yellow, flashing (Tx)

LON communication RS-485

Red, short flash (MODE)

During start-up; otherwise for future use

  • Automation Servers
  • Status LEDs