There are eight LEDs on the front panel of the Automation Server.
Function |
Color |
RS-485 A, Tx |
Yellow |
RS-485 A, Rx |
Green |
RS-485 B, Tx |
Yellow |
RS-485 B, Rx |
Green |
Ethernet, Link/Act/Speed |
Green/Yellow |
LON, Tx |
Yellow |
LON, Mode |
Red |
Status (Automation Server) |
Green/Red |
The Automation Server Ethernet and Status indicators comprise two LEDs (green/yellow and green/red respectively) in one structure. Normally, when one LED is lit, the other is not lit and vice versa, that is, the indicator will show one color at a time.
The LEDs indicate status of the Automation Server and the ongoing communication.
The SmartX server Status LED indicates the condition of the device.
LED Patterns |
Condition |
Green, constant |
Normal operation, status OK |
Green, flashing (~1 Hz) |
Device restarting, wait |
Red, constant |
Detected error, attention required |
Red, flashing (~1 Hz) |
Device operates, but a problem needs attention |
Red/green, flashing (~1 Hz) |
Firmware being downloaded, wait |
Red/green, vague |
Device firmware upgrade mode, wait |
No light |
No input power |
The RS-485 (COM A and COM B) LEDs indicate the condition of the RS-485 communication.
LED Patterns |
Condition |
Yellow, flashing (Tx) |
Transmit data |
Green, flashing (Rx) |
Receive data |
The Ethernet LED indicates the condition of the Ethernet communication.
LED Patterns |
Condition |
Green, flashing |
10 Mbit communication |
Yellow, flashing |
100 Mbit communication |
The LON LEDs indicate the condition of the LonWorks RS-485 communication.
LED Patterns |
Condition |
Yellow, flashing (Tx) |
LON communication RS-485 |
Red, short flash (MODE) |
During start-up; otherwise for future use |