earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AO-8, AO-V-8, DI-16, DO-FA-12, DO-FC-8, RTD-DI-16, UI-16, UI-8/AO-4, UI-8/AO-V-4, UI-8/DO-FC-4
Functionalities: Hardware
Product version: 2.0, 2.1, 3.0, 3.1, 3.2
9/7/2022

I/O Module LEDs

arrow1_rotationI/O Module Status LED arrow1_rotationI/O Channel Status LEDs

The I/O modules have the following status indicator LEDs on the front of the module:

  • I/O Module Status LED

  • I/O Channel Status LEDs

 
action_zoom_plus_stroke I/O module LEDs
Figure: I/O module LEDs

I/O Module Status LED

Each I/O module contains a green/red Status LED that indicates the status of the I/O module in relationship to the SmartX server. The LED is labeled Status and is located on the lower right side of the I/O Module placard.

The I/O module Status LED indicates the condition of the device.

Table: I/O Module Status LED Patterns

LED Patterns

Condition

Green, constant

Online and configured (at least one channel/point downloaded successfully)

Green, constant

Red, flashing (for 100 ms every 2 s)

Online and configured

Disabled Hand-Off-Auto (HOA) override switches

Applies only to I/O modules with HOA override switches and with manufacturing date earlier than 2021-W26 and upgraded with firmware version 2.017 or later. For more information, see Important Information on Central IO Modules with Manufacturing Date Earlier Than 2021-W26 .

Green, flashing (200 ms ON, 200 ms OFF)

Online and unconfigured (physical module that either matches/mismatches logical module)

Green, slow flashing (approximately every 3 s)

Low power mode (saves energy)

Red, constant

Error requiring attention (for example, the input voltage is too low)

Red, flashing (100 ms ON, 100 ms OFF)

Offline with respect to the SmartX server (both configured and unconfigured modules)

Red/Green, flashing (green 100 ms, red 100 ms)

Bootloader mode (downloading data)

No light

No input power

I/O Channel Status LEDs

Each digital input (DI) channel, digital output (DO) channel, and Universal Input (UI) channel contains a green I/O channel status LED. This LED indicates the On/Off state of the digital input or output.

You can also configure I/O channel status LEDs as an invert, so that either a HIGH or LOW voltage level can turn the LED ON.

Note:

For Universal Inputs, the I/O Channel Status LED is active only if the channel is configured as a digital input or as a counter input.

  • I/O Modules
  • Status LEDs