earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Security
Product version: 2024, 7.0
12/3/2024

Certificates Tab

Use the Certificates tab to manage certificates.

 
action_zoom_plus_stroke Certificates tab
Figure: Certificates tab

Table: Certificates Tab

Property

Description

Server

Select the server.

DNS/IP Address

Displays the server’s DNS or IP address.

Active Certificate

Displays the server’s active certificate.

Server

Displays the name and location of the selected server.

Address

Displays the DNS address or the IP address to the selected server.

Server Certificate

Displays available and active certificates for the selected servers.

From Certificate Store

Select to display certificates stored in Windows trusted storage.

For more information, see Windows Certificate Store for Enterprise Server and Enterprise Central .

Show Certificate

Click to display the active certificate.

Document Signature Certificate

Displays available and active certificated used for signing PDF notification reports. For more information, see Document Signature Certificate .

From Certificate Store

Select to display certificates stored in Windows trusted storage.

For more information, see Windows Certificate Store for Enterprise Server and Enterprise Central .

Show Certificate

Click to display the active certificate.

Manage Certificate

Click to open the Manage Certificates dialog box. For more information, see Manage Certificates Dialog Box .

  • Certificates
  • Document Signature Certificate
  • Adding a Certificate using WorkStation
  • Generating a Certificate Using WorkStation
  • Activating a Certificate Using WorkStation
  • Removing a Certificate Using WorkStation
  • Signing a PDF Notification Report with a Certificate
  • Manage Certificates Dialog Box
  • Windows Certificate Store for Enterprise Server and Enterprise Central