earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 安全
产品版本: 2023
2022/12/17

Adding a Security Banner 

You add a security banner to your system to notify the user that the user is entering a secure system.

显示更多
action_close

A security banner is displayed when a user enters a secure system. The security banner notifies the user of the legal rights connected to the use of the information in the secure system.

The banner is displayed for all users that enter the system regardless of their domains or rights and regardless of if they enter using WorkStation or WebStation.

重要:

WebStation users are logged off from WebStation when they reload a page if they are a member of a group where the group members are automatically logged off and the security banner is displayed.

To add a security banner
  1. In WorkStation, in the System Tree pane, select the EcoStruxure BMS server you want to configure.

  2. Click the Control Panel tab.

  3. Click Security settings .

  4. In Security settings - Control Panel, under Display security banner , click On .

  5. Click Edit banner .

  6. Type the text you want to display in the security banner.

  7. Click OK .

  8. Click the Save button

     
    action_zoom_plus_stroke
    .

  • Security Banner 
  • Control Panel Tab
  • Security Settings – Control Panel
  • Edit Banner – Dialog Box