Produits : WebStation
Fonctionnalités : Fonctionnalité de base
Version produit : 2024, 7.0
03/12/2024

Adding a Property to the Watch Pane in WebStation

You can monitor a property by adding it to the Watch pane.

Afficher plus
action_close

You add objects to the Watch pane to monitor their live values.

For example, you can monitor the impact of a change you are about to make in your system. Property changes are immediately displayed in the Watch pane.

You can save the Watch pane with all its objects and properties so that you can use it again the next time you log on to WebStation.

To add a property to the Watch Pane
  1. In WebStation, in the Watch pane toolbar, click Add .

  2. Select the property.

  3. Click OK .

  • Watch Pane in WebStation
  • Watch Pane – WebStation
  • Adding a Property to the Watch Pane from the Properties Dialog Box
  • Removing a Property from the Watch Pane in WebStation
  • Saving the Watch Pane in WebStation