earth_america
user_standard Zaloguj się
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Poradnik

Poradnik


Produkty: WebStation
Funkcje: Podstawowa funkcjonalność
Wersja produktu: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2018-05-18

Removing a Property from the Watch Pane in WebStation

You remove properties that you do not want to monitor from the Watch pane.

Pokaż więcej
action_close

You add objects to the Watch pane to monitor their live values.

For example, you can monitor the impact of a change you are about to make in your system. Property changes are immediately displayed in the Watch pane.

You can save the Watch pane with all its objects and properties so that you can use it again the next time you log on to WebStation.

To remove a property from the Watch Pane in WebStation
  • In WebStation, in the Watch pane, click X to the right of the property.

  • Watch Pane in WebStation
  • Watch Pane – WebStation
  • Adding a Property to the Watch Pane in WebStation
  • Saving the Watch Pane in WebStation