Use the Installation tab to edit the system installation information. The Schneider Electric partner or branch user cannot edit information if the system is associated to the end-user.
Property |
Description |
Site type |
Select the system type. If there is only one SmartStruxure server installed at the site, select Single site option. If there is more than one Enterprise Server installed at the site, select Multi site option. |
Site/building name |
Type the site/building name where the system is installed. |
Site company name |
Type the company name where the system is installed. |
System transition (if applicable) |
Select the legacy systems that existed on the site before installing Building Operation System. |
System application |
Select the applications to which the system is commissioned for. |
Segment/application |
Select the business segments you belong to. |
Installation address |
Type the site/building address where the system is installed. |
Country |
Type the country to which site/building belongs. |
State/province |
Type the state/province to which site/building belongs. |
City |
Type the city to which site/building belongs. |
Zip/postal code |
Type the zip/postal code of the region where site is located. |
Submit |
Click to update the system installation information. |
Cancel |
Click to leave this page without making any changes. |