Use the Features dialog box to select the .NET Framework 3.5.1 features for installation. The features are required for the WebReports installation, and it is recommended that you install the services before you install SQL Server.
Component |
Description |
.NET Framework 3.5.1 Features
|
Select to install all .NET Framework 3.5.1. Features. |
.NET Framework 3.5.1 |
Select to install .NET Framework 3.5.1. |
WCF Activation |
Select to install Windows Communication Foundation (WCF) Activation components. |
HTTP Activation |
Select to install HTTP Activation (applications that use HTTP Activation can start and stop dynamically in response to work items transmitted over the network using HTTP). |
Non-HTTP Activation |
Select to install Non-HTTP Activation (applications that use Non-HTTP Activation can start and stop dynamically in response to work items transmitted over the network using either Message Queuing, TCP, or named pipes). |