earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: WebReports
功能: 报告
产品版本: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
2021/12/16

Features Dialog Box for Windows Server 2008

Use the Features dialog box to select the .NET Framework 3.5.1 features for installation. The features are required for the WebReports installation, and it is recommended that you install the services before you install SQL Server.

 
action_zoom_plus_stroke Features dialog box
图: Features dialog box

表格: Features Dialog Box

Component

Description

.NET Framework 3.5.1 Features 

Select to install all .NET Framework 3.5.1. Features.

.NET Framework 3.5.1

Select to install .NET Framework 3.5.1.

WCF Activation

Select to install Windows Communication Foundation (WCF) Activation components.

HTTP Activation

Select to install HTTP Activation (applications that use HTTP Activation can start and stop dynamically in response to work items transmitted over the network using HTTP).

Non-HTTP Activation

Select to install Non-HTTP Activation (applications that use Non-HTTP Activation can start and stop dynamically in response to work items transmitted over the network using either Message Queuing, TCP, or named pipes).

  • Windows Roles and Features