earth_america
user_standard Connexion
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Comment faire pour

Comment faire pour


Produits : AS-B, AS-P, WorkStation, Project Configuration Tool
Fonctionnalités : Fonctionnalité de base
Version produit : 3.3, 2022
04/02/2022

Duplicating an Automation Server Using Restore 

You duplicate an EcoStruxure BMS server from a backup set using Restore when you want to reuse configuration data from a backup set in a standalone automation server.

Déclaration

The locally stored backup set and the automation server need to have the same password.

Restoring with new ID does not work if the database contains a BACnet interface.

Afficher plus
action_close

You can use the Restore function to re-use the configuration data from a backup set in a new standalone automation server. Rather than manually configuring your preferred automation server configuration, you can save time and configure the standalone automation server from a backup set.

The backup set used can originate from an automation server that is or has been part of a multi-server configuration.

To store a backup set in another location, you save a selected backup set to a folder on your WorkStation PC or network drive.

Pour plus d'informations, voir Backup Sets .

Protocol compatibility

The restore function to re-use configuration data from a backup set is supported for all protocols supported by EcoStruxure Building Operation software, except for BACnet and b3 BACnet.

LonWorks devices Neuron IDs deleted on duplicated automation server

The LonWorks devices connected to the automation server are not the same as the LonWorks devices that are to be connected to the duplicate. When you create a duplicate from an automation server, all Neuron IDs in the duplicate are deleted. This is also a way to avoid network conflicts.

After you created the duplicate, you add new Neuron IDs to the duplicate. You then commission all LonWorks devices on the new automation server.

Pour plus d'informations, voir LonWorks Device Workflows .

Password deleted on duplicated EcoStruxure BMS device

When you duplicate a SpaceLogic device from a backup set all passwords are deleted on the duplicate for security reasons. The only exception is the default admin password. The administrator is forced to change the password at the first logon at the duplicate. All users must be given new passwords by the administrator.

Multi-server site

To create a new automation server in a multi-server configuration, using a locally stored backup set, you need to make the backup set available for restore on the multi-server system. You add a new automation server to the Enterprise Server and select the backup set in the Create Object Wizard.

Pour plus d'informations, voir Creating an Automation Server from a Backup Set .

Standalone automation server site

You use a locally stored backup set to duplicate another automation server configuration in a standalone automation server. You then import the backup set to a client and restore to the new standalone automation server.

Pour plus d'informations, voir Duplicating an Automation Server Using Restore  .

Duplicate Automation Server from a Backup Set Workflow

Use the following workflow to duplicate an automation server from a backup set.

 
action_zoom_plus_stroke Duplicate Automation Server using restore flowchart
Figure : Duplicate Automation Server using restore flowchart
Backup an automation server

Backup an automation server that has the configuration you want to use in the new standalone automation server.

Pour plus d'informations, voir Backing Up EcoStruxure BMS Servers Manually .

Copy backup set to local directory

Copy the backup set to a local directory.

Pour plus d'informations, voir Saving an Automation Server Backup Set to Another Location .

Log on to standalone automation server

Log on to a new standalone automation server.

Pour plus d'informations, voir Connexion à WorkStation en tant qu'utilisateur EcoStruxure Building Operation .

Import backup set

Import the backup set.

Pour plus d'informations, voir Importing a Backup Set to Automation Server .

Restore automation server using Restore configuration with new IDs

Use the Restore configuration with new IDs function to duplicate the configuration data from the imported backup set in the new standalone automation server. The communication settings from the backup set are not duplicated.

Pour plus d'informations, voir Duplicating an Automation Server Using Restore  .

Déclaration

When you restore a standalone automation server, you are logged off and need to log on manually after the restore is complete.

To duplicate an automation server using restore
  1. In WorkStation, in the System Tree pane, select the server where you want to duplicate configuration data from a backup set.

  2. On the Actions menu, click Restore .

  3. In the Restore Options dialog box, in the Available restore points list, select the backup set.

  4. Select Restore configuration with new IDs checkbox to re-use the configuration data from the backup set in a new standalone automation server.

  5. Click Restore .

  6. Click Yes .

  7. Click Close .

  • Duplicate Automation Server from a Backup Set
  • Restore
  • Restore Options Dialog Box
  • Importing a Backup Set to Automation Server
  • Backup Set Text is Red