earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
用户界面

用户界面


产品: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
功能: 安全
产品版本: 2023
2022/12/17

Generate Certificate Dialog Box

Use the Generate Certificate dialog box to generate a self-signed certificate.

 
action_zoom_plus_stroke Generate certificate dialog box
图: Generate certificate dialog box

表格: Generate Certificate Dialog Box

Component

Description

Name

Enter the name of the certificate.

Description

Enter a description of the certificate.

Common name

Enter the certificates common name

Use IP/DNS from communication settings

Select to use the IP address or the DNS address from the communication settings in the EcoStruxure BMS server.

Email address

Enter the email address to the the person responsible for the certificate.

Organizational unit

Enter the organizational unit responsible for the certificate.

Organization

Enter the organization responsible for the certificate.

Locality

Enter the location of the organization or person who is responsible for the certificate.

Country

Select the country.

Valid from

Displays the date from when the certificates is valid. This date is always the current date.

Valid to

Enter the last date the certificate is valid.

  • Certificates
  • Generating a Certificate Using WorkStation