earth_america
user_standard Iniciar sessão
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interface de utilizador

Interface de utilizador


Produtos: AS-B, Enterprise Central, Enterprise Server, AS-P, Project Configuration Tool
Funcionalidades: Funcionalidade básica
Versão do produto: 3.2, 3.3, 2022
15-10-2020

Connect Agent Settings - Basic Tab

Use the Basic dialog box to configure the settings of Connect Agent to enable transfer of crash information of the EcoStruxure BMS servers to the Connect storage server.

 
action_zoom_plus_stroke Basic tab
Imagem: Basic tab

Tabela: Basic Tab

Component

Description

Enable crash information transfer

Select True to enable the Connect Agent service to transfer crash information to the Connect storage server.

  • Connect Agent Overview
  • Connect Agent Settings - Advanced Tab