earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: Automation Server, AS-B, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Basic Functionality
Product version: 1.8, 1.9
10/12/2017

Connect Agent Settings - Advanced Tab

Use the Advanced tab to configure the advanced settings of Connect Agent.

 
action_zoom_plus_stroke Advanced tab
Figure: Advanced tab

Table: Advanced Tab

Component

Description

Days between transfers

Select how often you want the Connect Agent to transfer the system data to the Connect storage server.

Maximum bandwidth

Select the bandwidth at which the system information is to be transfered. If '0' is selected, the system information is transfered at maximum bandwidth.

  • Connect Agent
  • Connect Agent Settings - Basic Tab